Das Unternehmen wurde 1961 gegründet und hat seinen Hauptsitz in Schwarzenburg. Seit 2011 ist Gilgen Door Systems Mitglied der japanischen Nabtesco Gruppe. Der Name Gilgen steht für innovative Antriebs- und Gesamtlösungen im Bereich der Tür-, Tor- und Wandsysteme. Schweizer Qualität, konsequente Präzision und ein internationales Netzwerk machen Gilgen Door Systems und seine weltweit über 1000 Mitarbeitenden zum verlässlichen Partner in nahezu jedem Land dieser Erde.
The Saxon bank "Sächsische Aufbaubank" of the Free State of Saxony provides fundings for companies, research institutes, as well as housing construction and urban development enerprises. A publicly accessible forest of concrete columns is located in front of the transparently designed building. The access from the underground car park to the staircase in the basement proves that sliding doors play a decisive role in the entrance experience. Function and design perfectly complement each other in the bi-parting version with glazed side door panels and glazed overhead panel. The low-profile sliding door has been executed in an elegant golden shade and serves as a porch system to prevent unpleasant draughts. It is equipped with a low-noise, long-life and automatic door locking system with mechanical manual unlocking on the inside. The door position and locking are monitored by the system. The installation was carried out on exposed concrete, which required extremely precise and neat work.